Read/Write |
About Dynamic Uncertainty |
Description |
Sets and returns the ON/OFF state which determines if the calibration that is about to be performed will support Dynamic Uncertainty for S-Parameters (Opt. 015). Dynamic Uncertainty for S-Parameters is supported ONLY for calibrations on standard S-Parameter channels. Calibrations performed with that feature enabled do NOT support the use of ALL traditional Guided calibration commands. These existing commands are used for the performing of the calibration: These commands might also optionally be used in performing the cal: |
VB Syntax |
guidedCal.UncertaintyEnabled = value |
Variable |
(Type) - Description |
|
guidedCal |
An GuidedCalibration Object |
|
value |
(Boolean) Enable state. Choose from: True - The next calibration initialized for the channel will support Dynamic Uncertainties for S-Parameters. False - The next calibration initialized for the channel will NOT support Dynamic Uncertainties for S-Parameters. |
Return Type |
Boolean |
Default |
False |
Examples |
guided.UncertaintyEnabled = True |
C++ Syntax |
HRESULT get_UncertaintyEnabled(VARIANT_BOOL* pState); HRESULT put_UncertaintyEnabled(VARIANT_BOOL state); |
Interface |
IGuidedCalibration11 |