Specifies settings and fixturing for Balanced Measurements.
|
CALCulate:FSIMulator |
Click a blue keyword to view the command details.
See Also
CALCulate<cnum>:FSIMulator:SNP:EXTRapolate <bool>
|
(Read-Write) Turns ON and OFF SNP file extrapolation for both 2-port and 4-port embedding/de-embedding. Learn more. Note: This command affects ALL measurements on the specified channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
Choose from: ON or 1 - Turns Extrapolation ON OFF or 0 - Turns Extrapolation OFF |
|
Examples |
CALC:FSIM:SNP:EXTR 1 |
|
Query Syntax |
CALCulate<cnum>:FSIMulator:SNP:EXTRapolate? |
|
Return Type |
Boolean |
|
OFF |
|
CALCulate<cnum>:FSIMulator:STATe <bool>
|
(Read-Write) Turns all three fixturing functions (de-embedding, port matching, impedance conversion) ON or OFF for all ports on the specified channel. Does not affect port extensions. Note: This command affects ALL measurements on the specified channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
Choose from: ON or 1 - Turns Fixturing ON OFF or 0 - Turns Fixturing OFF |
|
Examples |
CALC:FSIM:STAT 1 |
|
Query Syntax |
CALCulate<cnum>:FSIMulator:STATe? |
|
Return Type |
Boolean |
|
OFF |
|
Last Modified:
|
4-Nov-2013 |
Fixed link |
|
16-Nov-2010 |
Added extrapolate |