Controls the limit segments used for pass / fail testing.
|
CALCulate:LIMit: | DELete DISPlay | [STATe] SEGMent | AMPLitude | STARt | STOP | COUNt? | STIMulus | STARt | STOP | TYPE SOUNd | [STATe] |
Click on a keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
|
(Read-Write) Sets data for limit segments. |
|||||||||||
|
Parameters |
|
||||||||||
|
<cnum> |
Channel number of the measurement for which limit lines are to be set. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
||||||||||
|
<block> |
Data for all limit segments in REAL,64 format. The following is the data format for 1 segment:
|
||||||||||
|
Examples |
The following writes three max limit segments for a bandpass filter. CALC:LIM:DATA 1,3e5,4e9,-60,0,1,4e9,7.5e9,0,0,1,7.5e9,9e9,0,-30 |
||||||||||
|
Query Syntax |
CALCulate<cnum>:LIMit:DATA? |
||||||||||
|
Return Type |
Depends on FORM:DATA - All 100 predefined limit segments are returned. |
||||||||||
|
100 limit segments - all values set to 0 |
|||||||||||
|
(Write-only) Deletes all limit line data for the selected measurement on the specified channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC2:LIM:DATA:DEL |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
(Read-Write) Turns the display of limit segments ON or OFF (if the data trace is turned ON). |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<ON | OFF> |
ON (or 1) - turns the display of limit segments ON. |
|
Examples |
CALC:LIM:DISP:STAT ON |
|
Query Syntax |
CALCulate<cnum>:LIMit:DISPlay[:STATe]? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
ON |
|
|
(Read-only) Returns the Pass / Fail status of the limit line test. Returns 1 (Fail) if any data point fails for any limit segment. Limit display (CALC:LIM:DISP) does NOT have to be ON. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:LIM:FAIL? |
|
Return Type |
Boolean
|
|
Not Applicable |
|
|
(Read-Write) Sets the start (beginning) of the Y-axis amplitude (response) value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number between: -500 and 500 Display value is limited to the Maximum and Minimum displayed Y-axis values. |
|
Examples |
CALC:LIM:SEGM1:AMPL:STAR 10 |
|
Query Syntax |
CALCulate<cnum>:LIMit:SEGMent<snum>AMPLitude:STARt? |
|
Return Type |
Numeric |
|
0 |
|
|
(Read-Write) Sets the stop (end) of the Y-axis amplitude (response) value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number between: -500 and 500 Display value is limited to the Maximum and Minimum displayed Y-axis values. |
|
Examples |
CALC:LIM:SEGM1:AMPL:STOP 10 |
|
Query Syntax |
CALCulate<cnum>:LIMit:SEGMent<snum>AMPLitude:STOP? |
|
Return Type |
Numeric |
|
0 |
|
|
(Read-only) Returns the number of segments used in a limit test. All segments are counted, whether they are on or not. |
|
|
Parameters |
Not Applicable |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:LIM:SEGM:COUN? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
(Read-Write) Sets the start (beginning) of the X-axis stimulus value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number within the X-axis span of the analyzer. |
|
Examples |
CALC:LIM:SEGM1:STIM:STAR 10 |
|
Query Syntax |
CALCulate<cnum>:LIMit:SEGMent<snum>STIMulus:STARt? |
|
Return Type |
Numeric |
|
0 |
|
|
(Read-Write) Sets the stop (end) of the X-axis stimulus value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number within the X-axis span of the analyzer. |
|
Examples |
CALC:LIM:SEGM1:AMPL:STOP 10 |
|
Query Syntax |
CALCulate<cnum>:LIMit:SEGMent<snum>STIMulus:STOP? |
|
Return Type |
Numeric |
|
0 |
|
|
(Read-Write) Sets the type of limit segment. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<snum> |
Segment number. Choose any number between: |
|
<char> |
Choose from: LMIN - a MIN limit segment. Any response data below the MIN value will fail. OFF - the limit segment (display and testing) is turned OFF. |
|
Examples |
CALC:LIM:SEGM:TYPE LMIN |
|
Query Syntax |
CALCulate<cnum>:LIMit:SEGMent<snum>:TYPE? |
|
Return Type |
Character |
|
OFF |
|
|
(Read-Write) Turns limit testing fail sound ON or OFF. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<ON | OFF> |
ON (or 1) - turns sound ON. |
|
Examples |
CALC:LIM:SOUN ON |
|
Query Syntax |
CALCulate<cnum>:LIMit:SOUNd[:STATe]? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
|
(Read-Write) Turns limit segment testing ON or OFF.
|
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<ON | OFF> |
ON (or 1) - turns limit testing ON. |
|
Examples |
CALC:LIM:STAT ON |
|
Query Syntax |
CALCulate<cnum>:LIMit:STATe? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
Last Modified:
|
10-Jan-2011 |
Minor edits |
|
31-Oct-2008 |
Added Delete and Fail commands (8.33) |