Controls and queries settings that affect the PNA system.
| 
 SYSTem:COMMunicate: GPIB | PMETer | ADDRess | RDEVice | CLOSe | OPEN | READ? | RESet | WBINary | WBLock | WRITe VISA | RDEVice | CLOSe | FIND? | OPEN | READ? | RESet | TIMeout | WBINary | WRITe  | 
Click on a keyword to view the command details.
See Also
| 
 Note: This command is replaced with SYST:COMM:PSENsor (Read-Write) Specifies the GPIB address of the power meter to be used in a source power calibration. When performing a source power cal, the PNA will search VISA interfaces that are configured in the Keysight IO LIbraries on the PNA.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <num>  | 
 GPIB address of the power meter. Choose any integer between 0 and 30.  | 
| 
 Examples  | 
 SYST:COMM:GPIB:PMET 13 system:communicate:gpib:pmeter:address 14  | 
| 
 Query Syntax  | 
 SYSTem:COMMunicate:GPIB:PMETer[:ADDRess]?  | 
| 
 Return Type  | 
 Numeric  | 
| 
 13  | 
|
| 
 (Write only) Closes the remote GPIB session. This command should be sent when ending every successful OPEN session.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 Session identification number that was returned with the OPEN? command.  | 
| 
 Examples  | 
|
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Read-Write) Initiates a GPIB pass-through session. First send this OPEN command, then send the OPEN query to read the session ID number. An existing GPIB pass-through session remains open after an instrument preset. To learn more about GPIB pass-through capability, see the example program.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <bus>  | 
 Bus ID number. You can find the USB-GPIB adapter bus number by looking at the dialog that appears when the USB-GPIB device is connected. Error 1073 indicates the bus or address number is incorrect. Use 0 (zero) when connected using a GPIB cable to the PNA controller port.  | 
| 
 <addr>  | 
 GPIB Address of the device to be controlled  | 
| 
 <timeout>  | 
 The amount of time (in milliseconds) to wait for a response from the remote device after sending a command. A "timeout" error is displayed after this time has passed without a response.  | 
| 
 Examples  | 
|
| 
 Query Syntax  | 
 SYSTem:COMMunicate:GPIB:RDEVice:OPEN? Returns the session identification number that is used when communicating with this device.  | 
| 
 Return Type  | 
 Numeric  | 
| 
 Not Applicable  | 
|
| 
 (Read-only) Returns data from the GPIB pass-through device.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 Session identification number that was returned with the OPEN? command.  | 
| 
 Examples  | 
|
| 
 Return Type  | 
 String  | 
| 
 Not Applicable  | 
|
| 
 (Write-only) Performs the same function as SYST:COMM:GPIB:RDEV:CLOS except that ALL pass-through sessions are closed.  | 
|
| 
 Examples  | 
 SYST:COMM:GPIB:RDEV:RES  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Write-only) Sends data to a GPIB pass-through device. This command requires a header that specifies the size of the data to be written. The header (described below) is not passed along to the device. Use this command if too many embedded quotes prevent you from using SYST:COMM:GPIB:RDEV:WRIT. Use SYST:COMM:GPIB:RDEV:OPEN to open the pass through session.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 Session identification number that was returned with the OPEN? command.  | 
| 
 <data>  | 
 Data to be sent to the GPIB pass-through device. Use the following syntax: #<num digits><byte count><data bytes><NL><END> <num_digits> specifies how many digits are contained in <byte_count> <byte_count> specifies how many data bytes will follow in <data bytes>  | 
| 
 Examples  | 
 SYSTem:COMMunicate:GPIB:RDEVice:WBINary 101,#17ABC+XYZ<nl><end> # - always sent before data. 1 - specifies that the byte count is one digit (7). 7 - specifies the number of data bytes that will follow, not counting <NL><END>. ABC+XYZ - Data block <nl><end> - always sent at the end of block data. 
 The following example sends a line feed at the end. SYST:COMM:GPIB:RDEV:WBIN 1,#210SYST:PRES<EOL> The <EOL> represents your linefeed character.  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Write-only) Same as SYSTem:COMM:GPIB:RDEV:WBIN (above) but the header IS passed along to the device. Use this command if too many embedded quotes prevent you from using SYST:COMM:GPIB:RDEV:WRIT.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 Session identification number that was returned with the OPEN? command.  | 
| 
 <data>  | 
 Data to be sent to the GPIB pass-through device. See previous command.  | 
| 
 Examples  | 
 See previous example.  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Write-only) Sends ASCII string data to the GPIB pass-through device. A line feed is NOT appended to the string data. To send a line feed, see the example in SYST:COMM:GPIB:RDEV:WBIN.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 Session identification number that was returned with the OPEN? command.  | 
| 
 <string>  | 
 Commands to be sent to the GPIB pass-through device.  | 
| 
 Examples  | 
|
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Read-only) Returns the LAN hostname that is visible in the Help, About Network Analyzer dialog box. Learn more. This is the same information that is visible on the LXI compliance dialog.  | 
|
| 
 Parameters  | 
 None  | 
| 
 Example  | 
 SYST:COMM:LAN:HOSTname?  | 
| 
 Return Type  | 
 String  | 
| 
 Not applicable  | 
|
| 
 This command replaces SYST:COMM:GPIB:PMET:ADDR. (Read-Write) Specifies the type and location of the power meter to be used in a source power calibration.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <char>  | 
 Type of power meter/ sensor. Choose from: 
  | 
| 
 <string>  | 
 For GPIB, address of the power meter. Choose any integer between 0 and 30. For USB, the ID string of the power meter or power sensor. Use SYST:COMM:USB:PMET:CAT? to see a list of ID strings of connected power meters and sensors. For LAN, the hostname or IP address of the power meter. For ANY, any VISA resource string or a visa alias.  | 
| 
 Examples  | 
 SYST:COMM:PSEN gpib, "14" system:communicate:psensor usb, "Keysight Technologies,U2000A,MY12345678" syst:comm:psen lan, "mymeter.Keysight.com" syst:comm:psen any, "TCPIP0::mymeter.Keysight.com::5025::SOCKET"  | 
| 
 Query Syntax  | 
 SYSTem:COMMunicate:PSENsor?  | 
| 
 Return Type  | 
 Character / String  | 
| 
 GPIB  | 
|
| 
 (Read-only) Returns the ID string of power meters / sensors that are connected to the PNA USB. Use the list to select a power sensor for a source power cal. These meter/sensor ID strings can NOT be used as the resource string for configuring a USB-based PMAR (SYST:CONF:EDEV:IOConfig).  | 
|
| 
 Parameters  | 
 
  | 
| 
 Examples  | 
 SYST:COMM:USB:PMET:CAT? system:communicate:usb:pmeter:catalog?  | 
| 
 Return Type  | 
 Comma-delimited strings. Two power sensor strings are separate by a semicolon.  | 
| 
 Not applicable  | 
|
| 
 (Read-only) Queries the TCP/IP port number to use for opening a TCP/IP socket control connection to the PNA. The control connection is used for two purposes: 
 The port number can range from 5000 to 5099. The PNA will skip over 5025 as it is being used for the primary socket connection. To detect an SRQ, your program sends the appropriate commands via the regular socket connection to set up for a SRQ event to occur the same sequence of commands as if you were sending them via GPIB. You write your program so that while your program is doing SCPI transactions on the standard socket connection, a second thread of execution in your program detects the SRQ on the control connection and responds to the event. When the SRQ event occurs, the PNA sends a SRQ +xxx/n message on the control connection (where /n is linefeed character, ASCII value 10 decimal). The xxx value in the SRQ +xxx/n string is the IEEE 488.2 status byte at the time the SRQ was generated. So listening for that on the control connection is how your program detects the event. If for your socket communication youre using a software API that provides for asynchronous communication via a callback mechanism (for example, if youre using Microsofts winsock API, or their .NET Socket class as in the example program below), in that case your listener execution thread is created implicitly for you so your program doesnt have to create one explicitly. Note: If this SCPI query is sent to the PNA via a SCPI parser other than a TCP/IP socket connection (for example, if sent via GPIB), the query is not applicable in that case and will return value of 0.  | 
|
| 
 Parameters  | 
 None  | 
| 
 Example  | 
|
| 
 Return Type  | 
 Integer  | 
| 
 Not applicable  | 
|
| 
 (Write only) Closes the specified remote VISA session. VISA sessions should always be closed when you are finished communicating with the remote device. Use this command to close (end) each VISA session that was opened successfully using the OPEN command. If you have more than one open session, and need to close them all at the same time, it may be faster and easier to use the RESet command.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 VISA session number (see SYST:COMM:VISA:RDEV:OPEN[?]).  | 
| 
 Examples  | 
 SYST:COMM:VISA:RDEV:CLOS 1 system:communicate:visa:rdevice:close 2  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Read-only) Returns a comma separated list of either VISA address strings or aliases.  | 
|||||||||||||||||||
| 
 Parameters  | 
 
  | 
||||||||||||||||||
| 
 <VISA regex>  | 
 (String) VISA regular expressions are expressions defined by the user to find devices that have been set up on the VISA interface. The following are examples of VISA regular expressions: 
 Note that using "INSTR" in the VISA regular expression finds "instruments." To search all interfaces, use "?*".  | 
||||||||||||||||||
| 
 <ADDRess|ALIas>  | 
 Optional. Determines whether addresses or aliases are returned. Note: The list of aliases may have less‒or more‒entries than the list of addresses because not all addresses will have aliases, and one address can have more than one alias.  | 
||||||||||||||||||
| 
 Examples  | 
 SYST:COMM:VISA:RDEV:FIND? "?*",ADDR system:communicate:visa:rdevice:find? '?*INSTR',alias  | 
||||||||||||||||||
| 
 Return Type  | 
 Variant  | 
||||||||||||||||||
| 
 Addresses returned if no return-type specified  | 
|||||||||||||||||||
| 
 (Read-Write) Initiates a VISA pass-through session for a device. Immediately after successfully sending this command, send an OPEN? query to retrieve the unique session ID that is to be used whenever communicating with the device. Pass-through sessions can be closed by using the CLOSe command, the RESet command, or by properly shutting down the instrument or the analyzer application. Presetting the instrument will not close existing pass-through sessions. Note: When opening a socket session (addresses of type: “TCPIP[board]::host address::port::SOCKET”) , you must use the appropriate VISA Address for the <addr> argument. Using an alias to open a socket session is not currently supported. Aliases are allowed for all other types of supported sessions.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <addr>  | 
 VISA Address or alias name of the device to be controlled  | 
| 
 <timeout>  | 
 The amount of time (in milliseconds) to wait for a response from the remote device after sending a command. A "timeout" error is displayed after this time has passed without a response.  | 
| 
 Examples  | 
 SYST:COMM:VISA:RDEV:OPEN 'TCPIP0::A-N5242A-10096::hislip1::INSTR',1000 system:communicate:visa:rdevice:open 'MyAliasName',7000  | 
| 
 Query Syntax  | 
 SYSTem:COMMunicate:VISA:RDEVice:OPEN? Returns the VISA session identification number to be used when communicating with this device.  | 
| 
 Return Type  | 
 Numeric  | 
| 
 Not Applicable  | 
|
| 
 (Read-only) Returns data from the VISA pass-through device.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 VISA session number (see SYST:COMM:VISA:RDEV:OPEN[?]).  | 
| 
 Examples  | 
 SYST:COMM:VISA:RDEV:READ? 1 system:communicate:visa:rdevice:read? 3  | 
| 
 Return Type  | 
 String  | 
| 
 Not Applicable  | 
|
| 
 (Write-only) Closes all currently open VISA pass-through sessions. See also CLOSe to close only one session at a time.  | 
|
| 
 Examples  | 
 SYST:COMM:VISA:RDEV:RES  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Read-Write) Sets or returns the timeout value (in milliseconds) for VISA pass-through commands for the specified VISA session ID.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 VISA session number that was returned with the OPEN? command.  | 
| 
 <timeout>  | 
 The amount of time (in milliseconds) to wait for a response from the remote device after sending a command. A "timeout" error is displayed after this time has passed without a response.  | 
| 
 Examples  | 
 SYST:COMM:VISA:RDEV:TIM 1,6000 system:communicate:visa:rdevice:timeout 3,6000  | 
| 
 Query Syntax  | 
 SYSTem:COMMunicate:VISA:RDEVice:TIMeout? <ID> Returns the timeout value for the specified session ID.  | 
| 
 Return Type  | 
 Numeric  | 
| 
 2000  | 
|
| 
 (Write-only) Sends data to a VISA pass-through device. This command requires a header that specifies the size of the data to be written. The header (described below) is not passed along to the device.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 VISA session number (see SYST:COMM:VISA:RDEV:OPEN[?]).  | 
| 
 <data>  | 
 Data to be sent to the VISA pass-through device. Use the following syntax: #<num digits><byte count><data bytes><NL><END> <num_digits> specifies how many digits are contained in <byte_count> <byte_count> specifies how many data bytes will follow in <data bytes>  | 
| 
 Examples  | 
 SYSTem:COMMunicate:VISA:RDEVice:WBINary 1,#17ABC+XYZ<nl><end> # - always sent before data. 1 - specifies that the byte count is one digit (7). 7 - specifies the number of data bytes that will follow, not counting <NL><END>. ABC+XYZ - Data block <nl><end> - always sent at the end of block data. 
 The following example sends a line feed at the end. SYST:COMM:VISA:RDEV:WBIN 1,#210SYST:PRES<EOL> The <EOL> represents your linefeed character.  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|
| 
 (Write-only) Sends ASCII string data to the VISA pass-through device. If sending a command that returns data, follow with the READ? query.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ID>  | 
 VISA session number (see SYST:COMM:VISA:RDEV:OPEN[?]).  | 
| 
 <string>  | 
 Commands to be sent to the VISA pass-through device.  | 
| 
 Examples  | 
 SYST:COMM:VISA:RDEV:WRIT 1,'*IDN?' system:communicate:visa:rdevice:write 2,'SYST:PRES'  | 
| 
 Query Syntax  | 
 Not Applicable  | 
| 
 Not Applicable  | 
|