Controls the power delivered to the DUT.
SOURce: Multi-Dimensional Sweep - More commands POWer | ALC:MODE | CATalog? | AUTO | CENTer | COUPle | DETector | [LEVel] | SLOPe | STATe | MODE | PORT | STARt | STOP | SPAN | STARt | STOP |
Click on a keyword to view the command details.
See Also
(Read-only) Returns a list of valid port names that can be controlled. Some ports only have string names, NOT numbers. All commands that require a port argument have provisions for specifying either a port number OR a string name. See also: Remotely Specifying a Source Port. |
|
Parameters |
|
Examples |
SOUR:CAT? 'Some
PNA-X models return |
Return Type |
Comma-separated list of strings. |
Not applicable |
|
(Read-Write) Sets and returns the ALC mode for the specified channel and port. Use SOUR:POW:ALC:MODE:CAT? to return a list of valid ALC modes for the PNA. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<port> |
Source port number of the PNA. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<char> |
ALC Mode. For the PNA-X choose from:
To set Leveling Mode to Receiver Leveling, use the Receiver Leveling commands. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC INT source2:power2:alc:mode openloop source:power:alc:mode openloop,"Port 1 Src2" |
Query Syntax |
SOURce<cnum>:POWer<port>:ALC:MODE? [src] |
Return Type |
Character |
INTernal |
|
(Read-only) Returns a list of valid ALC modes for the specified channel and port number. Use the returned values to set SOUR:POW:ALC:MODE. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<port> |
Source port number of the PNA. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:CAT? source2:power2:alc:mode:catalog? source:power:alc:mode:catalog? "Port 1 Src2" |
Return Type |
Comma-separated list of strings. |
Not applicable |
|
(Read-Write) Sets the attenuation level for the selected channel. Sending this command turns automatic attenuation control (SOUR:POW:ATT:AUTO) to OFF. If the ports are coupled, changing the attenuation on one port will also change the attenuation on all other ports. To turn port coupling OFF use SOURce:POWer:COUPle OFF. Note: Attenuation cannot be set with Sweep Type set to Power See Sens:Power:ATT to change receiver attenuation. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<port> |
Source port number of the PNA. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<num> |
Attenuation value. The range of settable values depends on the PNA model. To determine the valid settings, do one of the following:
If an invalid attenuation setting is entered, the PNA will select the next lower valid value. For example, if 19 is entered, then for an E8361A, 10 dB attenuation will be selected. Note: This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ATT 10 source2:power2:attenuation maximum source:power:att 20, "Port 1 Src2" |
Query Syntax |
SOURce<cnum>:POWer<port>:ATTenuation? [min/max] [src] [min/max,src] |
Return Type |
Numeric |
0 |
|
(Read-Write) Turns automatic attenuation control ON or OFF. Setting an attenuation value (using SOURce:POWer:ATTenuation <num>) sets AUTO OFF. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
<port> |
Source port number of the PNA. If unspecified, value is set to 1.To make settings for ports that are not simple numbers, use the [src] argument. |
<bool> |
ON (or 1) - turns coupling ON. The analyzer automatically selects the appropriate attenuation level to meet the specified power level. OFF (or 0) - turns coupling OFF. Attenuation level must be set using SOURce:POWer:ATTenuation <num>. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW2:ATT:Auto On source2:power:attentuation:auto off sour:pow:att:auto 1, "Port 1 Src2" |
Query Syntax |
SOURce<cnum>:POWer:ATTenuation:Auto? [src] |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
|
(Read-Write) Sets the power sweep center
power. Must also set: |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<num> |
Center power. Actual achievable leveled power depends on frequency. |
<port> |
If provided, this argument is ignored by the PNA. |
Examples |
SOUR:POW:CENT
-15 |
Query Syntax |
SOURce<cnum>:POWer:CENTer? |
Return Type |
Numeric |
0 dBm |
|
(Read-Write) Turns Port Power Coupling ON or OFF. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<ON | OFF> |
ON (or 1) - turns coupling ON. The same power level is used for both source ports. OFF (or 0) - turns coupling OFF. Power level can be set individually for each source port. |
Examples |
SOUR:POW:COUP
ON |
Query Syntax |
SOURce<cnum>:POWer:COUPle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
|
(Read-Write) The PNA models with external leveling are now OBSOLETE. Sets the source leveling loop as Internal or External. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<char> |
INTernal - Internal leveling is applied to the source EXTernal - External leveling is applied to the source through a rear-panel connector. ONLY provided on 3 GHz, 6 GHz, and 9 GHz PNA models. |
Examples |
SOUR:POW:DET
INT |
Query Syntax |
SOURce<cnum>:POWer:DETector? |
Return Type |
Character |
INTernal |
|
(Read-Write) Sets the RF power output level. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<port> |
Source port number of the PNA. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<num> |
Source power in dBm. Note: The range of settable power values depends on the PNA model and if source attenuators are installed. To determine the range of values, perform a query using MAX, then MIN, as an argument. (SOUR:POW:ATT:AUTO must be set to ON) Example: SOURce:POWer? Max Actual achievable leveled power depends on frequency. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW1
5 sour:pow 5, "Port 1 Src2" |
Query Syntax |
SOURce<cnum>:POWer[:LEVel][:IMMediate][:AMPLitude]? [src] |
Return Type |
Numeric |
0 dBm |
|
(Read-Write) Sets the RF power slope value. Also enable the slope state using SOUR:POW:SLOP:STAT ON. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<num> |
Slope value in db/GHz. Choose any value between -2 and 2 (0 is no slope). |
<port> |
If provided, this argument is ignored by the PNA. |
Examples |
SOUR:POW:SLOP .5234434 source2:power:level slope -1.345 |
Query Syntax |
SOURce<cnum>:POWer[:LEVel]:SLOPe? |
Return Type |
Numeric |
0 |
|
(Read-Write) Turns Power Slope ON or OFF. Set the slope using SOUR:POW:SLOP. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<ON|OFF> |
ON (or 1) - turns slope ON. OFF (or 0) - turns slope OFF. |
<port> |
If provided, this argument is ignored by the PNA. |
Examples |
SOUR:POW:SLOP:STAT ON |
Query Syntax |
SOURce<cnum>:POWer[:LEVel]:SLOPe:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
|
(Read-Write) Sets the state of PNA source for the specified port. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<port> |
Source port number of the PNA. If unspecified, <port> is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<state> |
Source state. Choose from:
|
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:MODE ON source2:power4:mode OFF sour:pow:mode on, "Port 1 Src2" |
Query Syntax |
SOURce<cnum>:POWer<port>:MODE? [src] |
Return Type |
Character |
Auto |
|
(Read-Write) Sets and reads the power sweep start power value for a specific port. This allows uncoupled forward and reverse power sweep ranges. Must also set SENS:SWE:TYPE POWer and SOUR:POW:COUPle OFF. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<port> |
Source port number of the PNA. If unspecified, <port> is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<num> |
Start power in dBm. Note: The range of settable power values depends on the PNA model and if source attenuators are installed. To determine the range of values, perform a query using MAX, then MIN, as an argument. (SOUR:POW:ATT:AUTO must be set to ON) Example: SOURce:POWer:STARt? MIN Actual achievable leveled power depends on frequency. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW1:PORT:STAR
-15 |
Query Syntax |
SOURce<cnum>:POWer<port>:PORT:STARt? [src] |
Return Type |
Numeric |
-10 dBm |
|
(Read-Write) Sets and reads the power sweep stop power value for a specific port. This allows uncoupled forward and reverse power sweep ranges. Must also set SENS:SWE:TYPE POWer and SOUR:POW:COUPle OFF. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<port> |
Source port number of the PNA. If unspecified, <port> is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<num> |
Stop power in dBm. Note: The range of settable power values depends on the PNA model and if source attenuators are installed. To determine the range of values, perform a query using MAX, then MIN, as an argument. (SOUR:POW:ATT:AUTO must be set to ON) Example: SOURce:POWer:STARt? MIN Actual achievable leveled power depends on frequency. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW1:PORT:STOP
-15 |
Query Syntax |
SOURce<cnum>:POWer<port>:PORT:STOP? [src] |
Return Type |
Numeric |
0 dBm |
|
(Read-Write) Sets the power sweep span power. Must also set: |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
<num> |
Span power. Actual achievable leveled power depends on frequency. |
<port> |
If provided, this argument is ignored by the PNA. |
Examples |
SOUR:POW:SPAN
-15 |
Query Syntax |
SOURce<cnum>:POWer:SPAN? |
Return Type |
Numeric |
0 dBm |
|
(Read-Write) Sets the power sweep start power for ALL ports being used by the specified channel. Must also set: SENS:SWE:TYPE POWer and SOURce:POWer:STOP <num>. To set start power for a specific port, use SOUR:POW:PORT:STARt. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<num> |
Start power. Note: The range of settable power values depends on the PNA model and if source attenuators are installed. To determine the range of values, perform a query using MAX, then MIN, as an argument. (SOUR:POW:ATT:AUTO must be set to ON) Example: SOURce:POWer:STARt? MIN Actual achievable leveled power depends on frequency. |
<port> |
If provided, this argument is ignored by the PNA. |
Examples |
SOUR:POW:STAR
-15 |
Query Syntax |
SOURce<cnum>:POWer:STARt? |
Return Type |
Numeric |
0 dBm |
|
(Read-Write) Sets the power sweep stop power for ALL ports being used by the specified channel.. Must also set: SENS:SWE:TYPE POWer and SOURce:POWer:START <num>. To set start power for a specific port, use SOUR:POW:PORT:STOP. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<num> |
Stop power. Note: The range of settable power values depends on the PNA model and if source attenuators are installed. To determine the range of values, perform a query using MAX, then MIN, as an argument. (SOUR:POW:ATT:AUTO must be set to ON) Example: SOURce:POWer:STOP? MAX Actual achievable leveled power depends on frequency. |
<port> |
If provided, this argument is ignored by the PNA. |
Examples |
SOUR:POW:STOP -15 source2:power:stop -7 |
Query Syntax |
SOURce<cnum>:POWer:STOP? |
Return Type |
Numeric |
0 dBm |
|