This example does the following in separate subprograms:
Setup Uncertainty Manager Workspace
Perform a standard 2-port Guided Cal
Perform a Cable Characterization
Perform a Noise Characterization
Perform a 2-Port Uncertainty Cal
Make Uncertainty Trace Settings
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file, such as Notepad, and save it on the PNA hard drive as *.vbs.
Learn how to setup and run the macro.
See all Dynamic Uncertainty commands
Learn about Dynamic Uncertainty (Option 015)
See Other SCPI Example Programs
|
Dim app Dim scpi ' Create / Get the PNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser 'Preset the analyzer scpi.Parse "SYST:PRESet" SetupWorkspace TwoPortGuidedCal PerformCableChar PerformNoiseChar TwoPortUncertCal MakeTraceSettings '********************************************* ' Setup Uncertainty Workspace ' Sub SetupWorkspace cableCatalog = scpi.Parse("SYSTem:UNCertainty:CABLe:CATalog?") ' Strip the leading and trailing quotation ' marks from the catalog string cableCatalog = Mid(cableCatalog, 2, Len(cableCatalog) - 3) ' Tokenize the comma-delimited list string ' into an array of the individual substrings cables = Split(cableCatalog, ",") ' Re-assemble the cable list into one string delimited by linefeed characters cableCatalog = "" For i = 0 To UBound(cables) cableCatalog = cableCatalog & cables(i) & Chr(10) ' Uncomment the following line to reset (clear) repeatability data for the cable 'scpi.Parse "SYSTem:UNCertainty:CABLe:REPeat:RESet '" & cables(i) & "'" Next MsgBox "Cables:" & Chr(10) & Chr(10) & cableCatalog portCatalog = scpi.Parse("SOURce:CATalog?") ' Strip the leading and trailing quotation ' marks from the catalog string portCatalog = Mid(portCatalog, 2, Len(portCatalog) - 3) ' Tokenize the comma-delimited list string ' into an array of the individual substrings ports = Split(portCatalog, ",") portCatalog = "" For i = 0 To UBound(ports) portNum = i + 1 ' Ensuring we only count the actual testports and not any source-only ports like external sources If (ports(i) = "Port " & CStr(portNum)) Then cable = scpi.Parse("SYSTem:UNCertainty:PORT" & CStr(portNum) & ":CABLe:SELect?") portCatalog = portCatalog & ports(i) & ": " & cable & Chr(10) ' Uncomment the following line to reset (clear) noise data for the port 'scpi.Parse "SYSTem:UNCertainty:PORT" & CStr(portNum) & ":NOISe:RESet" End If Next MsgBox "Port Cables:" & Chr(10) & Chr(10) & portCatalog ' Uncomment the following line to select the particular cable for all ports 'scpi.Parse "SYSTem:UNCertainty:PORT:CABLe:ALL:SELect '" & cables(0) & "'" ' Uncomment the following line to copy the noise data for Port 1 to be used for all ports 'scpi.Parse "SYSTem:UNCertainty:PORT:NOISe:ALL:COPY 1" ' Uncomment the following line to reset (clear) the noise data for all ports 'scpi.Parse "SYSTem:UNCertainty:PORT:NOISe:ALL:RESet" ' The next lines toggle uncertainty manager properties on scpi.Parse "SYSTem:UNCertainty:ETERm:NOISe:ENABle ON" MsgBox "Noise enabled for cals = " & scpi.Parse("SYSTem:UNCertainty:ETERm:NOISe:ENABle?") scpi.Parse "SYSTem:UNCertainty:ETERm:CABle:REPeat:ENABle ON" MsgBox "Cable repeatability enabled for cals = " & scpi.Parse("SYSTem:UNCertainty:ETERm:CABle:REPeat:ENABle?") scpi.Parse "SYSTem:UNCertainty:ETERm:SDEFinitions:ENABle ON" MsgBox "Standards definition uncertainties enabled for cals = " & scpi.Parse("SYSTem:UNCertainty:ETERm:SDEFinitions:ENABle?") ' Uncomment the following line to change the max number of uncertainty points for cals to be 500 'scpi.Parse "SYSTem:UNCertainty:POINts:MAXimum 500" MsgBox "Max number of uncertainty points for cals = " & scpi.Parse("SYSTem:UNCertainty:POINts:MAXimum?") ' Perform a Save of the currently loaded uncertainty workspace ('.ml4') file scpi.Parse "SYSTem:UNCertainty:STORe" ' Uncomment the following line to save the currently loaded uncertainty workspace to a specific ('.ml4') filename 'scpi.Parse "SYSTem:UNCertainty:STORe 'myUncertaintyWorkspace.ml4'" ' Uncomment the following line to recall the uncertainty workspace ('.ml4') file that we just saved 'scpi.Parse "SYSTem:UNCertainty:LOAD 'myUncertaintyWorkspace.ml4'" End Sub '********************************************* ' Measure the steps of a cable characterization, ' noise characterization, or a calibration. Sub MeasureStepsOfCharacterizationOrCal(isNoiseCharacterization, numSteps) Dim retVal Dim opc For i = 1 To numSteps step = "Step " + CStr(i) + " of " + CStr(numSteps) ' A "connection adjustment" means the user has to change something about the connection, ' such as wiggling cable and re-connecting standard during a repeatability characterization, ' or to move the slide position of a sliding load if a connection step in a calibration ' were to involve a sliding load. If isNoiseCharacterization = False Then numConnectionAdjustmentsPerStep = scpi.Parse("sens1:corr:coll:guid:iter:min? " + CStr(i)) Else ' noise characterization ' in this case, "iterations" are just repetitive measurements, not re-adjust/re-measure the standard numConnectionAdjustmentsPerStep = 1 End If For j = 1 To numConnectionAdjustmentsPerStep strPrompt = scpi.Parse("sens1:corr:coll:guid:desc? " + CStr(i)) retVal = MsgBox(strPrompt, vbOKCancel, step) If retVal = vbCancel Then WScript.Quit opc = scpi.Parse("sens1:corr:coll:guid:acq STAN" + CStr(i) + ";*OPC?") Next Next scpi.Parse "sens1:corr:coll:guid:save" End Sub Function FormatList(list) Dim tokens ' Strip the leading and trailing quotation ' marks from the list string list = Mid(list, 2, Len(list) - 3) ' Tokenize the comma-delimited list string ' into an array of the individual substrings tokens = Split(list, ",") ' Using Trim to remove leading and trailing spaces. For i = 0 To UBound(tokens) tokens(i) = Trim(tokens(i)) Next FormatList = tokens End Function '********************************************* ' Performing a NON-UNCERTAINTY Guided 2-port cal (Ports 1 and 2) Sub TwoPortGuidedCal Dim connList Dim connIndex1, connIndex2 Dim kitList Dim kitIndex Dim message Dim formattedConnListStr message = "A non-uncertainty 2-port calibration will now be performed, " message = message & "because a calibration is needed for characterizing the cables" MsgBox message ' Query the list of connectors that the PNA system recognizes connList = scpi.Execute("sens:corr:coll:guid:conn:cat?") ' Turn the list from comma-delimited string into an array of strings connList = FormatList(connList) message = "Enter the index number (from this list) of your DUT connector for Port 1:" & Chr(10) & Chr(10) ' Note: the array's indexing is 0-based but the numbering is being presented in the InputBox as 1-based For i = 0 To UBound(connList) formattedConnListStr = formattedConnListStr & Chr(9) & CStr(i+1) + ") " & connList(i) & Chr(10) Next connIndex1 = InputBox(message & formattedConnListStr) If connIndex1 = "" Then WScript.Quit ' Convert number from String to Long and from 1-based index to 0-based connIndex1 = CLng(connIndex1) - 1 scpi.Execute "sens:corr:coll:guid:conn:port1 '" & connList(connIndex1) & "'" message = "Enter the index number (from this same list again) of your DUT connector for Port 2:" & Chr(10) & Chr(10) connIndex2 = InputBox(message & formattedConnListStr) If connIndex2 = "" Then WScript.Quit ' Convert number from String to Long and from 1-based index to 0-based connIndex2 = CLng(connIndex2) - 1 scpi.Execute "sens:corr:coll:guid:conn:port2 '" & connList(connIndex2) & "'" ' Note: If your PNA has more than 2 ports, then uncomment ' one or both of these next two lines. 'scpi.Execute "sens:corr:coll:guid:conn:port3 ""Not used"" " 'scpi.Execute "sens:corr:coll:guid:conn:port4 ""Not used"" "
' This next block of commented code demonstrates how to specify an adapter ' and it's electrical delay, in situations where you are performing an ' Unknown Thru or Adapter Removal calibration. In most situations, the ' PNA is able to correctly determine an adapter's electrical length ' at the end of the calibration. However, there are scenarios where ' the PNA cannot correctly calculate the length -- such as when the channel ' has a relatively small number of measurement points (for example, 201 or less) ' and the adapter is significantly long (for example, a cable that is several feet). ' In these cases, the ADAP commands (below) enable you to explicitly specify ' the adapter you are using. ' Send these commands prior to the "sens:corr:coll:guid:init" command. ' Create adapter and return the adapter number 'adapterNum = scpi.Execute("sens:corr:coll:guid:adap:cre? '" & connList(connIndex1) & "','"& connList(connIndex2) & "'") ' The adapterNum string contains a '+' character. ' Here we convert to integer to remove that. 'adapterNum = CStr( CInt(adapterNum) ) ' Specify that this adapter has 10 nanoseconds electrical delay (coaxial). 'scpi.Execute "sens:corr:coll:guid:adap" & adapterNum & ":del 10E-9" ' Text description of adapter 'scpi.Execute "sens:corr:coll:guid:adap" & adapterNum & ":desc 'My adapter'" ' Select to use this adapter specifically between ports 1 and 2 'scpi.Execute "sens:corr:coll:guid:adap" & adapterNum & ":path 1,2" ' End of adapter block
' Query the list of acceptable cal kits and ' ECal module characterizations for Port 1. kitList = scpi.Execute("sens:corr:coll:guid:ckit:cat? '" & connList(connIndex1) & "'") ' Turn the list from a comma-delimited string into an array kitList = FormatList(kitList) ' Select the Cal Kit or ECal module characterization to use for Port 1. message = "Enter the index number (from this list) of your cal kit or ECal module characterization for Port 1:" message = message & Chr(10) & Chr(10) For i = 0 To UBound(kitList) message = message & Chr(9) & CStr(i+1) + ") " & kitList(i) & Chr(10) Next kitIndex = InputBox(message) If kitIndex = "" Then WScript.Quit ' Convert number from String to Long and from 1-based index to 0-based kitIndex = CLng(kitIndex) - 1 scpi.Execute "sens:corr:coll:guid:ckit:port1 '" & kitList(kitIndex) & "'" ' Query the list of acceptable cal kits ' and ECal module characterizations for Port 2. kitList = scpi.Execute("sens:corr:coll:guid:ckit:cat? '" & connList(connIndex2) & "'") ' Turn the list from a comma-delimited string into an array kitList = FormatList(kitList) ' Select the Cal Kit or ECal module characterization to use for Port 2. message = "Enter the index number (from this list) of your cal kit or ECal module characterization for Port 2:" message = message & Chr(10) & Chr(10) For i = 0 To UBound(kitList) message = message & Chr(9) & CStr(i+1) + ") " & kitList(i) & Chr(10) Next kitIndex = InputBox(message) If kitIndex = "" Then WScript.Quit ' Convert number from String to Long and from 1-based index to 0-based kitIndex = CLng(kitIndex) - 1 scpi.Execute "sens:corr:coll:guid:ckit:port2 '" & kitList(kitIndex) & "'" ' This determines whether the cal will be a "Guided Power Cal" ' or just a traditional S-parameter cal. message = "On which port number shall power be measured? " message = message & "For a traditional guided cal without power cal, enter 0" Dim powerPort powerPort = CInt( InputBox(message) ) If powerPort > 0 Then scpi.Execute("sens:corr:coll:guid:psen" & CStr(powerPort) & ":stat on") Dim retVal retVal = MsgBox("Is the power sensor's connector type or gender different from the DUT connector for that port?", vbYesNo) If retVal = vbYes Then message = "Enter the index number of your power sensor's connector. Choose from this list:" & Chr(10) & Chr(10) ' Select the sensor's connector. connIndex1 = InputBox(message & formattedConnListStr) If connIndex1 = "" Then WScript.Quit connIndex1 = CLng(connIndex1) - 1 scpi.Execute "sens:corr:coll:guid:psen" & CStr(powerPort) & ":conn '" & connList(connIndex1) & "'" ' Query the list of acceptable cal kits and ECal module characterizations ' that are applicable for the sensor's connector. kitList = scpi.Execute("sens:corr:coll:guid:ckit:cat? '" & connList(connIndex1) & "'") ' Turn the list from comma-delimited string into an array of strings kitList = FormatList(kitList) ' Select the Cal Kit or ECal module characterization to use for de-embed of the sensor's connector. message = "Enter index number of your cal kit or ECal module characterization to use for de-embed of the sensor's connector. " message = message & "Choose from this list:" & Chr(10) & Chr(10) For i = 0 To UBound(kitList) message = message & Chr(9) & CStr(i+1) + ") " & kitList(i) & Chr(10) Next kitIndex = InputBox(message) If kitIndex = "" Then WScript.Quit kitIndex = CLng(kitIndex) - 1 scpi.Execute "sens:corr:coll:guid:psen" & CStr(powerPort) & ":ckit '" & kitList(kitIndex) & "'" Else scpi.Execute("sens:corr:coll:guid:psen" & CStr(powerPort) & ":conn 'Ignored'") End If ' End of block that considers the sensor's connector ' Ask for the power level to perform the power cal at ' (if this command is omitted, the default is 0 dBm). Dim powerLevel powerLevel = InputBox("Enter the power level for the power cal to be performed at") If powerLevel = "" Then Exit Sub scpi.Execute "sens:corr:coll:guid:psen" & CStr(powerPort) & ":pow:lev " & powerLevel Else scpi.Execute("sens:corr:coll:guid:psen1:stat off") End If ' End of block that considers if the cal will include power calibration
' This next block of commented code ' shows optional functions when using ECal. ' Send these "sens:corr:pref" commands prior to the ' "sens:corr:coll:guid:init" command. ' Read ECAL information from ECal module #1 on the USB bus ' about the Keysight factory characterization data 'module1Info = scpi.Execute("sens:corr:coll:ckit:inf? ECAL1,CHAR0") 'MsgBox "Description of ECal Module #1:" & Chr(10) & Chr(10) & module1Info
' The following command enables auto orientation of ' the ECal module (The PNA senses which port of the ' module is connected to which port of the PNA). 'scpi.Execute "sens:corr:pref:ecal:ori ON" ' However, if you are measuring at very low power levels where ' the PNA may fail to sense the module's orientation, then turn auto ' orientation OFF and specify how the module is connected. ' "A1,B2" indicates Port A of the module is connected ' to PNA Port 1 and Port B is connected to PNA Port 2). 'scpi.Execute "sens:corr:pref:ecal:ori OFF" 'scpi.Execute "sens:corr:pref:ecal:pmap ECAL1,'A1,B2'" ' End of optional ECal setup
' Initiate the calibration and query the number of steps scpi.Execute "sens:corr:coll:guid:init" numCalSteps = CLng(scpi.Execute("sens:corr:coll:guid:steps?")) MsgBox "Number of steps is " + CStr(numCalSteps) ' Measure the standards and conclude the cal MeasureStepsOfCharacterizationOrCal False, numCalSteps MsgBox "The cal needed for the cable repeatability characterizations is done" End Sub '********************************************* ' Perform Cable Characterization Sub PerformCableChar ' Select/activate the default (S11) measurement that should still ' be present since a Preset preceded this subroutine scpi.Parse "CALC1:PAR:SEL 'CH1_S11_1'" ' Ensure the previously-performed calibration is turned on for that selected measurement scpi.Parse "CALC1:CORR ON" ' Initiate repeatability characterizations on Channel 1 for Ports 1 and 2, with 3 ' iterative measurements of each standard (normally users should specify more than 3 ' iterations per standard but it just makes this example speedier) Dim numRequestedIterations numRequestedIterations = 3 ' Begin characterization for port 1 scpi.Parse "sens1:corr:coll:guid:unc:char:cable 1, " + CStr(numRequestedIterations) Dim numCharSteps ' Query the number of connection steps numCharSteps = CLng(scpi.Parse("sens1:corr:coll:guid:steps?")) message = "Now to characterize the cable currently associated with port 1. " message = message & "Number of standard steps for characterizing port 1 cable = " & numCharSteps MsgBox message MeasureStepsOfCharacterizationOrCal False, numCharSteps MsgBox "Cable characterization for port 1 is done" ' Begin characterization for port 2 scpi.Parse "sens1:corr:coll:guid:unc:char:cable 2, " + CStr(numRequestedIterations) ' Query the number of connection steps numCharSteps = CLng(scpi.Parse("sens1:corr:coll:guid:steps?")) message = "Now to characterize the cable currently associated with port 2. " message = message & "Number of standard steps for characterizing port 2 cable = " & numCharSteps MsgBox message MeasureStepsOfCharacterizationOrCal False, numCharSteps MsgBox "Cable characterization for port 2 is done" End Sub '********************************************* 'Perform Noise Characterization Sub PerformNoiseChar ' Initiate noise characterization on Channel 1 for Ports 1 and 2, with 3 iterative ' measurements of each standard (normally users should specify more than 3 iterations ' per standard but it just makes this example speedier) scpi.Parse "sens1:corr:coll:guid:unc:char:noise 1, 2, 3" Dim numCharSteps ' Query the number of connection steps numCharSteps = CLng(scpi.Parse("sens1:corr:coll:guid:steps?")) message = "Now to characterize the system noise for ports 1 and 2. " message = message & "Number of connection steps to be made = " & numCharSteps MsgBox message MeasureStepsOfCharacterizationOrCal True, numCharSteps MsgBox "Noise characterization is done" End Sub
'********************************************* 'Perform 2-port Uncertainty Calibration (Ports 1 and 2) on Channel 1 Sub TwoPortUncertCal Dim kitList Dim kitIndex Dim message ' Specify this calibration is to be performed with uncertainties. scpi.Parse "sens1:corr:coll:guid:UNCertainty:ENABle ON" ' Query the list of uncertainty cal kits and ' ECal module factory characterizations applicable for the port cable connector. kitList = scpi.Parse("sens:corr:coll:guid:ckit:port1:cat?") ' Turn the list from comma-delimited string into an array of strings kitList = FormatList(kitList) message = "Now to perform an uncertainty calibration for ports 1 and 2. " message = message & "Enter the index number (from this list) of your cal kit or ECal module to use:" message = message & Chr(10) & Chr(10) ' Note: the array's indexing is 0-based but the numbering is being presented in the InputBox as 1-based For i = 0 To UBound(kitList) message = message & Chr(9) & CStr(i+1) + ") " & kitList(i) & Chr(10) Next ' Select the Cal Kit or ECal module to use for both ports. ' If the selected kit does not have a suitable set of standards ' that can mate the connector of the cable attached to Port 2, ' then the attempt to INIT the cal should yield an applicable error message. kitIndex = InputBox(message) If kitIndex = "" Then WScript.Quit ' Convert from String to Long and from 1-based index to 0-based kitIndex = CLng(kitIndex) - 1 scpi.Parse "sens:corr:coll:guid:ckit:port1 '" & kitList(kitIndex) & "'" scpi.Parse "sens:corr:coll:guid:ckit:port2 '" & kitList(kitIndex) & "'" ' Note: If your PNA has more than 2 ports, then uncomment ' one or both of these next two lines just in case this channel ' may have had a remote non-Uncert cal performed prior that ' involving port 3 and/or 4. 'scpi.Parse "sens:corr:coll:guid:conn:port3 """" " 'scpi.Parse "sens:corr:coll:guid:conn:port4 """" "
' This next block of commented code ' shows optional functions when using ECal. ' Send these "sens:corr:pref" commands prior to the ' "sens:corr:coll:guid:init" command. ' Read ECAL information from ECal module #1 on the USB bus ' about the factory characterization data 'module1Info = scpi.Parse("sens:corr:coll:ckit:inf? ECAL1,CHAR0") 'MsgBox "Description of ECal Module #1:" & Chr(10) & Chr(10) & module1Info
' The following command enables auto orientation of ' the ECal module (The PNA senses which port of the ' module is connected to which port of the PNA). 'scpi.Parse "sens:corr:pref:ecal:ori ON" ' However, if you are measuring at very low power levels where ' the PNA may fail to sense the module's orientation, then turn auto ' orientation OFF and specify how the module is connected. ' "A1,B2" indicates Port A of the module is connected ' to PNA Port 1 and Port B is connected to PNA Port 2). 'scpi.Parse "sens:corr:pref:ecal:ori OFF" 'scpi.Parse "sens:corr:pref:ecal:pmap ECAL1,'A1,B2'" ' End of optional ECal setup ' Initiate the calibration and query the number of steps scpi.Parse "sens:corr:coll:guid:init" numCalSteps = scpi.Parse("sens:corr:coll:guid:steps?") MsgBox "Number of steps is " + CStr(numCalSteps) ' Measure the standards and conclude the cal MeasureStepsOfCharacterizationOrCal False, numCalSteps MsgBox "Cal is done" End Sub '********************************************* 'Make Uncertainty Trace Settings Sub MakeTraceSettings ' Note: normally you would first ensure your active measurement is an S-parameter channel ' measurement before this point, and that the channel has an uncertainty cal to be ' able to turn on uncertainty display, but as the TwoPortUncertCal subroutine has ' executed right before this one, that is already ensured. chanNum = CInt(scpi.Parse("SYSTem:ACTive:CHANnel?")) If (chanNum = 0) Then MsgBox "No active channel" WScript.Quit End If activeMeasName = scpi.Parse("SYSTem:ACTive:MEASurement?") scpi.Parse "CALCulate" & CStr(chanNum) & ":PARameter:SELect " & activeMeasName MsgBox "Uncertainty Display Type = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:DISPlay:TYPE?") On Error Resume Next scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:DISPlay:TYPE SHADe" If Err.Number <> 0 Then MsgBox Err.Description Err.Clear Else MsgBox "Uncertainty Display Type = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:DISPlay:TYPE?") End If On Error GoTo 0 MsgBox "CoverageFactor = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:DISPlay:CFACtor?") ' Uncomment the following line to try setting the CoverageFactor = 3 'scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:DISPlay:CFACtor 3" scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:CABLe:REPeat OFF" MsgBox "Cable Repeatability Uncertainty state = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:CABLe:REPeat?") scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:CABLe:REPeat ON" MsgBox "Cable Repeatability Uncertainty state = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:CABLe:REPeat?") scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:NOISe OFF" MsgBox "Measurement Noise Uncertainty state = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:NOISe?") scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:NOISe ON" MsgBox "Measurement Noise Uncertainty state = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:NOISe?") scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:ETERm OFF" MsgBox "Error Term Uncertainty state = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:ETERm?") scpi.Parse "CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:ETERm ON" MsgBox "Error Term Uncertainty state = " & scpi.Parse("CALCulate" & CStr(chanNum) & ":UNCertainty:MODE:ETERm?") End Sub |