| Read only | About Path Configurator | 
| Description | Returns a handle to the specified PathElement object. Each element object contains a unique set of values. The Value Property is used to set the value for each element. This command is used to set both RF and IF Path Configuration. | 
| VB Syntax | Set elem = pathConfig.Element (element) | 
| Variable | (Type) - Description | 
| elem | (Object) IPathElement | 
| pathConfig | A PathConfiguration (object) | 
| element | (String) Configurable element. Use pathConfig.Elements to return a list of configurable elements or see a list of configurable elements for various VNA models. | 
| Return Type | Object | 
| Default | Not Applicable | 
| Examples | See examples: | 
| C++ Syntax | HRESULT Element( BSTR elemName, IPathElement** ppElement); | 
| Interface | IPathConfiguration |