| Write/Read | About Equal Tone Power | 
| Description | Note: This command is replaced with LevelingMethod Property Sets and returns the ON | OFF state of Equal Tone Power for the Swept IMD or IMSpectrum measurement. | 
| VB Syntax | object.EqualTonePower = value | 
| Variable | (Type) - Description | 
| object | A SweptIMD or IMSpectrum Object | 
| value | (Boolean) - Choose from: True - Set equal tone power. False - Do NOT set equal tone power. | 
| Return Type | Boolean | 
| Default | False | 
| Examples | ims.EqualTonePower = true 'Write | 
| value = imd.EqualTonePower 'Read | |
| C++ Syntax | HRESULT get_EqualTonePower(VARIANT_BOOL* val) HRESULT put_EqualTonePower(VARIANT_BOOL val) | 
| Interface | ISweptIMD2 IIMSpectrum2 |