About Frame Setup Modes

When to Select MAC PDU Mode

The MAC PDU mode focuses on the MAC PDU as the lowest-level component in configuring the frame. The generated waveforms are suitable for receiver test applications.

In the MAC PDU mode, you can:

When to Select Physical Mode

The Physical mode provides a quick method for configuring a spectrally correct waveform with user-selected data in the downlink or uplink bursts. In this mode, the software does not automatically generate an FCH that matches the frame configuration or automatically include broadcast messages in the waveform. The generated waveforms are suitable for component test applications.

In the Physical mode, you can:

Related Topics

MAC PDU mode:DL/UL example

Physical mode: DL example

Physical mode: UL example

Using the MAC Editor