:CGMemory:FILE:NAME
Command Syntax
:CGMemoryN:FILE:NAME "filename"
Where N identifies one of eight {1:8} color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:FILE:NAME?
Query Response
"string"
Description
Enters the name (including path) of a file to be imported into a color grade memory using the :CGMemory:FILE:LOAD command. If no path is given, the file expected to be in the default \Colorgrade-Grayscale folder.