:CGMemory:LOAD:SOURce

Command Syntax

:CGMemoryN:LOAD:SOURce <source_waveform>

Where N identifies one of eight {1:8} color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Where <source_waveform> can be one of the following:

  • CHANnel<connection1-8>_<ch1-8>; With connection 1, the "1_" part is optional, and you can simply use CHANnel<ch1-8>.
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:64}

Query Syntax

:CGMemory{1:8}:LOAD:SOURce?

Description

Selects the source waveform to load into color grade memory. Use the :CGMemory:LOAD command to actually load the selected source.

Example Command Sequence

:CGMemory2:LOAD:SOURce CHAN1_1
:CGMemory2:LOAD

Parent Command