:CGMemory:LOAD

Command Syntax

:CGMemoryN:LOAD

Where N identifies one of eight {1:8} color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Description

Loads the selected waveform source into the indicated eye-memory location. Use the :CGMemory:LOAD:SOURce command to select the source. Use the :CGMemory:DISPlay command to display the eye-memory waveform.

To load a color grade-gray scale file into color grade memory, use the :CGMemory:FILE:LOAD and :CGMemory:FILE:NAME commands.

Example Command Sequence

:CGMemory2:LOAD:SOURce CHAN1_1
:CGMemory2:LOAD
:CGMemory2:DISPlay ON

Child Commands