:CHANnel:ESCaling:OFFSet

Command Syntax

:CHANnelN:ESCaling:OFFSet <offset>

<offset> is a double.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:ESCaling:OFFSet?

Description

Enters or queries the offset setting for an external hardware (like a transducer, for example).

The offset units are the same as specified with the :CHANnel:ESCaling:UNITs command.

To apply external hardware compensation, use the :CHANnel:ESCaling:STATe command.