:CHANnel:ESCaling:STATe

Command Syntax

:CHANnelN:ESCaling:STATe {OFF | ON}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:ESCaling:STATe?

Description

Turns on and off compensation for external hardware (like a transducer, for example) in the test setup. This allows Infiniium to measure values and show vertical scaling as if the measurements were made before the external hardware rather than at the input to the oscilloscope channel.

The following table show the relationship between external hardware input, gain, and offset measurement units and the oscilloscope's displayed vertical scale.

Transducer Compensation Units
Transducer Measurement Units Oscilloscope
Vertical Scale/Division
Input Units Gain Conversion Factor Units Offset Units
VOLTs V/V V V/div
AMPere* V/A A A/div
WATT V/W W W/div
UNKown V/U# U U/div
*. Electrical channel only.
#. Unknown units.

See also :CHANnel:PROBe:ACCessories:ATTenuator:STATe.

Example

:CHANnel1_2:ESCaling:STATe ON