:CHANnel:ESCaling:UNITs
Command Syntax
:CHANnelN:ESCaling:UNITs {AMPere | VOLT | WATT | UNKNown}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:ESCaling:UNITs?
Description
Specifies the units for an external hardware's input signal.
To apply external hardware compensation, use the :CHANnel:ESCaling:STATe command.
Example
:CHANnel1_2:ESCaling:UNITs VOLT