:CMODe:SNDRatio:LFPDelay
Command Syntax
:CMODeN:SNDRatio:LFPDelay <number_of_UIs>
<number_of_UIs> is an integer.
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:SNDRatio:LFPDelay?
Description
This parameter is used in the filter to compute the linear fit pulse response. It is also a number of unit intervals (UIs). It is sometimes denoted using Dp.
Technology standard test documents typically tell you the value expected to be used for this parameter.