:CMODe:SNDRatio:SAVE

Command Syntax

:CMODeN:SNDRatio:SAVE {OFF | ON}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:SNDRatio:SAVE?

Description

When AUTomatic is selected as the SNDR standard (see :CMODe:SNDRatio:STANdard), this command lets you turn on or off saving of the automatically calculated Sigma-n locations to a standard definition file.

When saving the automatic calculations to a standards file is turned on, use the :CMODe:SNDRatio:SAVE:FILE command to specify the file name.