:CMODe:SNDRatio:NAVerages

Command Syntax

:CMODeN:SNDRatio:NAVerages <number_of_averages>

<number_of_averages> is an integer.

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:SNDRatio:NAVerages?

Description

Specifies the number of patterns to average in the SNDR linear fit computation.

Technology standard test documents typically tell you the value expected to be used for this parameter.