:CMODe:YBOTtom?
Query Syntax
:CMODeN:YBOTtom?
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Description
Queries the amplitude value represented by the graticule's bottom edge. To query the amplitude value represented by the graticule's top edge, use :CMODe:YTOP?. Use the :CMODe:YSCale command to set the amplitude scale (volts or Watts). Use the :CMODe:YOFFset command to set the amplitude offset.