:CMODe:YRANge
Command Syntax
:CMODeN:YRANge <scale>
<scale> is a double.
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:YRANge?
Description
Sets or queries the common-mode waveforms's vertical range. This is the vertical scale per division value (:CMODe:YSCale) multiplied by eight divisions.
Use the :CMODe:YOFFset command to change a channel's vertical offset.