:CMODe:YSCale:FINE
Command Syntax
:CMODeN:YSCale:FINE {{OFF | 0} | {ON | 1}}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:YSCale:FINE?
Query Response
{0 | 1}
Description
Enables or disables fine adjustment of the vertical scale.
When OFF (coarse adjustment), the vertical scale is adjusted in a 1-2-5 sequence.
When ON (fine adjustment), the vertical scale is adjusted in smaller, evenly spaced increments.