:CMODe:YOFFset

Command Syntax

:CMODeN:YOFFset <offset>

<offset> is a double.

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:YOFFset?

Description

Sets the voltage that is represented at the center of the display for the selected common-mode waveform.Offset parameters are vertical scale dependent. Currently, the offset can be expressed in volts only using the :CMODe:YUNits command. Use the :CMODe:YUNits command to change a channel's vertical scale.