*TRG (Trigger)

Command Syntax

*TRG

Description

Acquires data for the active waveform display, if the trigger conditions are met, according to the current settings. The *TRG common command has the same effect as the :ACQuire:RUN command.