*OPT? (Option)
Query Syntax
*OPT?
Description
Returns a comma-separated list of all packages, features, and options active (not expired) on the real-time oscilloscope, or Infiniium 2026 Offline. For example, "F-ASI,F-JIT" indicates "Advanced Signal Integrity Software (EQ, De-embedding)" and "Jitter and Phase Noise Analysis Software" licenses. The order of the comma-delimited fields within the string is random.
This same string can be returned by the ":SYSTem:OPTions? FRAMe" command.
Example Query Response
"F-ASI,F-JIT"
License String Fields
For more information about the packages, features, and options that can be returned, see: