*TST? (Hardware Self Tests)
Query Syntax
*TST?
Query Response
{0 | 1}
Description
Runs the instrument self-test, blocking until the test is complete. Return code of 0 indicates a pass, non-zero indicates failure.
If there is a failure, you can use the :SYSTem:TEST query to return the results of the most recent self-test.
You can cancel a running self test using the :SYSTem:TEST:CANCel command.