*SRE (Service Request Enable)

Command Syntax

*SRE <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

*SRE?

Description

Enters a decimal-weighted value in the service request enable register that masks the ability to report bits in the status byte event register. To read the status byte register, use the *STB common command. By setting the *SRE, when the event happens, you have enabled Infiniium interrupt capability. Infiniium will then do an SRQ (service request), which is an interrupt. The Service Request Enable Register contains a mask value for the bits to be enabled in the Status Byte Register. A "1" in the Service Request Enable Register enables the corresponding bit in the Status Byte Register. A "0" disables the bit.

Status Byte Register Commands
Register Read Write Command
Event ♦   *STB?
Enable (mask) ♦ ♦ *SRE
Status Byte Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
OPER RQS/MSS ESB MAV — MSG USR TRG
Enable
Register
               
Sets Sends a service request interrupt (SRQ) to the controller.

Bit Definitions

TRG
A true indicates that a trigger has occurred. This bit is set by the Trigger Event Register.
USR
A true indicates that an enabled user event condition has occurred. This bit is set by the User Event Register.
MSG
A true indicates that a message has been displayed and that the message queue has at least one entry. This bit is set by the Message Event Register.
MAV
A true indicates that an output message is ready.
ESB
A true indicates that an enabled event status condition occurred. This bit is set by the Standard Event Register.
RQS/MSS
A true indicates that Infiniium has requesting service.
OPER
A true indicates that enabled operation status conditions have occurred. This bit is set by the Operation Event Register.