:DIFF:YOFFset

Command Syntax

:DIFFN:YOFFset   <offset>

<offset> is a double.

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:YOFFset?

Description

Sets the voltage that is represented at the center of the display for the selected differential waveform.Offset parameters are vertical scale dependent. Currently, the offset can be expressed in volts only using the :DIFF:YUNits command. Use the :DIFF:YUNits command to change a channel's vertical scale.