:DIFF:YSCale:FINE

Command Syntax

:DIFFN:YSCale:FINE {{OFF | 0} | {ON | 1}}

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:YSCale:FINE?

Query Response

{0 | 1}

Description

Enables or disables fine adjustment of the vertical scale.

When OFF (coarse adjustment), the vertical scale is adjusted in a 1-2-5 sequence.

When ON (fine adjustment), the vertical scale is adjusted in smaller, evenly spaced increments.