:DIFF:YRANge

Command Syntax

:DIFFN:YRANge   <scale>

<scale> is a double.

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:YRANge?

Description

Sets or queries the differential waveform's vertical range. This is the vertical scale per division value (:DIFF:YSCale) multiplied by eight divisions.

Use the :DIFF:YOFFset command to change a channel's vertical offset.