Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:DISPlay:WINDow:IRESponse{N}:TOPMost

:DISPlay Time-Domain Windows Commands
  • :DISPlay:WINDow:TIME{N}:DMODe
  • :DISPlay:WINDow:TIME{N}:LEGend:EXPand
  • :DISPlay:WINDow:TIME{N}:LOCation
  • :DISPlay:WINDow:TIME{N}:TOPMost
  • :DISPlay:WINDow:TIME{N}:TSIGnal
  • :DISPlay:WINDow:IRESponse{N}:DMODe
  • :DISPlay:WINDow:IRESponse{N}:LEGend:EXPand
  • :DISPlay:WINDow:IRESponse{N}:LOCation
  • :DISPlay:WINDow:IRESponse{N}:TOPMost
  • :DISPlay:WINDow:IRESponse{N}:TSIGnal
  • :DISPlay:WINDow:SRESponse{N}:DMODe
  • :DISPlay:WINDow:SRESponse{N}:LEGend:EXPand
  • :DISPlay:WINDow:SRESponse{N}:LOCation
  • :DISPlay:WINDow:SRESponse{N}:TOPMost
  • :DISPlay:WINDow:SRESponse{N}:TSIGnal

Command Syntax

:DISPlay:WINDow:IRESponse{N}:TOPMost  {FUNCtion{1:64} | TRACe{1:128} }

{N} identifies a widow {1:4}.

Query Syntax

:DISPlay:WINDow:IRESponse{1:4}:TOPMost?

Description

When an Impulse Response waveform content window is displayed in tab tiled mode and there are multiple displayed waveforms, selects a waveform to display in the graticule area.

Sibling Commands

  • :DISPlay:WINDow:IRESponse{N}:DMODe
  • :DISPlay:WINDow:IRESponse{N}:LEGend:EXPand
  • :DISPlay:WINDow:IRESponse{N}:LOCation