:DISPlay:WINDow:TIME{N}:TSIGnal
Command Syntax
:DISPlay:WINDow:TIMEN:TSIGnal
Where N indicates one of four possible Waveform windows. For example, TIME1.
Query Syntax
:DISPlay:WINDow:TIMEN:TSIGnal?
Description
When a Waveform content window is displayed in overlapped mode and there are multiple displayed waveforms, selects a waveform to "bring to front" in the graticule area. Channel and differential channel waveforms can be viewed in a Waveform content window.