:DISPlay:WINDow:SRESponse{N}:DMODe

Command Syntax

:DISPlay:WINDow:SRESponse{N}:DMODe {OVERlapped | TILed | TTILed}

{N} identifies a widow {1:4}.

Query Syntax

:DISPlay:WINDow:SRESponse{1:4}:DMODe?

Description

Configures the layout of a Step Response waveform content window.

OERlapped (Overlapped Window)
All waveforms that are assigned to the window are displayed on top of each other.
TILed (Tiled Window)
Each waveform in the window is displayed in its own graticule. This selection is available whenever more that one waveform is assigned to a content window.
TTILed (Tab Tiled Window)
One waveform is displayed in the graticule and any remaining waveforms are shown in small windows along the bottom of the graticule. Use the :DISPlay:WINDow:SRESponse{N}:TOPMost command to select the waveform to place in the graticule.

Sibling Commands