:FUNCtion:PARameters:BUSer:CFILe:RELoad

Command Syntax

:FUNCtionN:PARameters:BUSer:CFILe:RELoad

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Reloads the XML configuration file for the selected user-defined function.

Use the :FUNCtion:PARameters:BUSer:CFILe parent command to configure the function.

Parent Command