:FUNCtion:PARameters:BUSer:LSTatus:REASon?
Query Syntax
:FUNCtion:PARameters:BUSer:LSTatus:REASon?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Returns the reason for a failed load of a configuration file.
Use the :FUNCtion:PARameters:BUSer:CFILe command to configure the function.