:FUNCtion:PARameters:BUSer:CFLoaded?

Query Syntax

:FUNCtionN:PARameters:BUSer:CFLoaded?

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Response

{1 | 0}

Description

Queries the existence of the specified user-defined operator. Returns a one if the operator is defined and a zero it the operator has not been setup.

Use the :FUNCtion:PARameters:BUSer:CFILe sibling command to configure the function.