:FUNCtion:PARameters:BUSer:LSTatus?

Query Syntax

:FUNCtion:PARameters:BUSer:LSTatus?

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Returns the status of the loading of the XML configuration file. Use the :FUNCtion:PARameters:BUSer:LSTatus:REASon? child command to return the reason for a failed load.

Use the :FUNCtion:PARameters:BUSer:CFILe sibling command to load the configuration file for the function.

Child Commands