:FUNCtion:PARameters:CONVolve:FMODel

Command Syntax

:FUNCtionN:PARameters:CONVolve:FMODel {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtion{1:64}:PARameters:CONVolve:FMODel?

Query Response

{1 | 0}

Description

Flips the S-parameters of an Apply s2p operator (:FUNCtion:FOPerator). If S-parameter file's data is not defined with the ports located as shown in the following diagram, flip the S-parameters to ensure that the S-parameter order is properly interpreted. Use the :FUNCtion:PARameters:CONVolve:FNAMe command to specify the S-parameter file.

Example Command Sequence

:FUNCtion2:FOPerator CONVolve
:FUNCtion2:PARameters:CONVolve:FNAMe "C:\Users<user_name>\Documents\Keysight\Infiniium\S-Parameter Data\DUT_4.s4p"
:FUNCtion2:PARameters:CONVolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:PARameters:CONVolve:PORDer PORDer1234  // Port order in file
:FUNCtion2:PARameters:CONVolve:PEXTract TPORt2  // Extract port data
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.