:FUNCtion:PARameters:CONVolve:NGAin
Command Syntax
:FUNCtionN:PARameters:CONVolve:NGAin {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtion{1:64}:PARameters:CONVolve:NGAin?
Query Response
{1 | 0}
Description
For an Apply s2p operator (:FUNCtion:FOPerator), this command turns on and off the Normalize Gain option. When selected (on), any DC gain is removed when applying s2p.