:FUNCtion:PARameters:CONVolve:FNAMe

Command Syntax

:FUNCtionN:PARameters:CONVolve:FNAMe "<path substitution string>\subfolder\filename"

Where:

  • N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
  • "<path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
  • "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\S-Parameter Data.
  • "filename" is a string without the filename extension.

Query Syntax

:FUNCtionN:PARameters:CONVolve:FNAMe?

Description

Specifies an S-parameter file that define a basic one-block model for an Apply s2p operator (:FUNCtion:FOPerator). These files use a filename extension of .s2p. Any time delay added by the S-parameter file will be automatically removed in order to align the input and output waveforms. Use the :FUNCtion:PARameters:CONVolve:FMODel command to flip the file's S-parameter data, if needed. Two commands are provided that allow you to use 4-port S-parameters files (.s4p) with this operator. The commands are :FUNCtion:PARameters:CONVolve:PEXTract and :FUNCtion:PARameters:CONVolve:PORDer. This command supports the DEFault common child command.

Default User Folder

The default folder for storing S-parameter files is in %USER_DATA_DIR%\S-Parameter Data as shown in this picture. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\S-Parameter Data\filename.

File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Default.

Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.

Example Command Sequence

:FUNCtion2:FOPerator CONVolve
:FUNCtion2:PARameters:CONVolve:FNAMe "%USER_DATA_DIR%\S-Parameter Data\DUT_4.s2p"
:FUNCtion2:PARameters:CONVolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.