:FUNCtion:PARameters:CONVolve:PORDer

Command Syntax

:FUNCtionN:PARameters:CONVolve:PORDer {PORDer1234 | PORDer1324}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:CONVolve:PORDer?

Description

Specifies the order of the S-parameter file's ports to ensure that the data is properly interpreted by an Apply s2p operator (:FUNCtion:FOPerator). The following table shows the relationship between the three commands used to define and extract the 2-port data from the S-parameter file.

The :FUNCtion:PARameters:CONVolve:PORDer and :FUNCtion:PARameters:CONVolve:PEXTract commands are only available after an 4-port S-parameter file has been opened using the :FUNCtion:PARameters:CONVolve:FMODel command.

Arguments and Dialog-Box Settings for 4-Port S-Parameters Files
Port Configuration
in s4p File
4 Port Numbering Argument
(PORDer)
2 Port Extraction Argument
(PEXTract)
Flip Model Argument
(FMODel)
PORDer1324
(1⇔2)TPORt1
(3⇔4)TPORt2
OFF
PORDer1234
(1⇔3)TPORt1
(2⇔4)TPORt2
OFF
PORDer1324
(1⇔2)TPORt1
(3⇔4)TPORt2
ON
PORDer1234
(1⇔3)TPORt1
(2⇔4)TPORt2
ON

Example Command Sequence

:FUNCtion2:FOPerator CONVolve
:FUNCtion2:PARameters:CONVolve:FNAMe "C:\Users<user_name>\Documents\Keysight\Infiniium\S-Parameter Data\DUT_4.s4p"
:FUNCtion2:PARameters:CONVolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:PARameters:CONVolve:PORDer PORDer1234  // Port order in file
:FUNCtion2:PARameters:CONVolve:PEXTract TPORt2  // Extract port data
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.