:FUNCtion:PARameters:DEMBed:BANDwidth

Command Syntax

:FUNCtionN:PARameters:DEMBed:BANDwidth <bandwidth>

<bandwidth> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DEMBed:BANDwidth?

Description

Specifies the bandwidth, in Hertz, of a 2-Port DeEmbedding operator (:FUNCtion:FOPerator). This minimizes the effects of noise.

The bandwidth is limited by the bandwidth set for the input channel or waveform. However, you are able to specify lower corner frequencies.

Use the :FUNCtion:PARameters:DEMBed:BLIMit command to select the type of bandwidth filter used. Use the :FUNCtion:PARameters:DEMBed:FNAMe command to open an existing network file that models your test setup.

Example Command Sequence

:FUNCtion2:FOPerator DEMBed
:FUNCtion2:PARameters:DEMBed:FNAMe "C:\Users<user_name>\Documents\Keysight\Infiniium\De-Embedding Networks\DUT_4.tf2"
:FUNCtion2:PARameters:DEMBed:BANDwidth 8.5E9
:FUNCtion2:PARameters:DEMBed:BLIMit BRICkwall
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.