:FUNCtion:PARameters:DEMBed:CFRequency
Command Syntax
:FUNCtionN:PARameters:DEMBed:CFRequency <center_frequency>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
<center_frequency> is a double.
Query Syntax
:FUNCtionN:PARameters:DEMBed:CFRequency?
Description
When the BANDpass filter type is selected (see :FUNCtion:PARameters:DEMBed:BLIMit), this command specifies the center frequency of the bandpass filter.