:FUNCtion:PARameters:DEMBed:NGAin

Command Syntax

:FUNCtionN:PARameters:DEMBed:NGAin {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtion{1:64}:PARameters:DEMBed:NGAin?

Query Response

{1 | 0}

Description

For a 2-Port DeEmbedding operator (:FUNCtion:FOPerator), this command turns on and off the Normalize Gain option. When selected (on), any DC gain of the transfer function is removed. This can be used when modeling probes.