:FUNCtion:PARameters:DEMBed:STEP
Command Syntax
:FUNCtionN:PARameters:DEMBed:STEP {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtion{1:64}:PARameters:DEMBed:STEP?
Query Response
{1 | 0}
Description
For a 2-Port DeEmbedding operator (:FUNCtion:FOPerator), this command turns on and off the Show Step Response option. When selected (on), the selected network file is automatically loaded into the S-Parameter/Transfer Function Viewer and a step response chart is added if the parameters can be determined; otherwise, you can add the chart by selecting the proper parameters. See :NETWorks:TRACe General Commands.