:GRAPh:SHERtz:X:AUToscale

Command Syntax

:GRAPh:SHERtzN:X:AUToscale

Where N specifies one of four {1:4} waveform content windows.

Description

Automatically scales the X-axis of the specified Seconds (Hz) waveform content window. Use the :GRAPh:SHERtz:X:CENTer, :GRAPh:SHERtz:X:SPAN, :GRAPh:SHERtz:X:STARt, and :GRAPh:SHERtz:X:STOP sibling commands to individually set these values.