:GRAPh:SHERtz:Y:AUToscale

Command Syntax

:GRAPh:SHERtzN:Y:AUToscale

Where N specifies one of four {1:4} waveform content windows.

Description

Automatically offsets and scales the Y-axis (time) of the specified Seconds (Hz) waveform content window. Use the :GRAPh:SHERtz:Y:OFFSet, and :GRAPh:SHERtz:Y:SCALe sibling commands to individually set these values.