:GRAPh:SHERtz:X:STARt

Command Syntax

:GRAPh:SHERtzN:X:STARt <frequency>

<frequency> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:SHERtzN:X:STARt?

Description

For the specified Seconds (Hz) waveform content window, sets the graph's X- axis start frequency in Hertz. Use the :GRAPh:SHERtz:X:AUToscale sibling command to automatically set the center, span, start, and stop settings. Use the :GRAPh:SHERtz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.