:GRAPh:SHERtz:Y:SCALe
Command Syntax
:GRAPh:SHERtzN:Y:SCALe <scale>
<scale> is a double.
Where N specifies one of four {1:4} waveform content windows.
Query Syntax
:GRAPh:SHERtzN:Y:SCALe?
Description
Sets the vertical scale of the specified Seconds (Hz) content window in seconds-per-division. The vertical expansion and contraction is referenced to the center graticule (:GRAPh:SHERtz:Y:OFFSet sibling command) of the display. Use the :GRAPh:SHERtz:Y:AUToscale sibling command to automatically set the offset and scale settings. Use the :GRAPh:SHERtz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.