:LLINe:HOFFset
Command Syntax
:LLINeN:HOFFset <offset>
Where N identifies one of 64 {1:64} possible limit lines. For example, :LLINe23.
<offset> is a double.
Query Syntax
:LLINeN:HOFFset?
Description
Specifies a horizontal offset in time for the selected Limit Line Test. All limit lines that are defined within the Limit Line Test are shifted by the specified time.
Example
:LLINe2:HOFFset 500E-12