:LLINe:LOAD:FNAMe

Command Syntax

:LLINeN:LOAD:FNAMe  "<path substitution string>\subfolder\filename"

Where:

  • N identifies one of 64 {1:64} possible limit lines. For example, :LLINe23.
  • "<path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
  • "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\Limit Lines.
  • "filename" is a string.

Query Syntax

:LLINeN:LOAD:FNAMe?

Description

Specifies the filename (*.lltx), path, and extension of the target limit-line file to load. After the file loads, you can display the limit line using the :LLINe:DISPlay sibling command.

Default User and Demo Folders

The default user data folder for storing limit-line files is in %USER_DATA_DIR%\Limit Lines as shown in this picture. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\Limit Lines\filename.

The default demo folders for loading limit-line files is in %DEMO_DIR%\Limit Lines\Demo as shown in the following picture. It is good practice to include a path substitution string with the subfolders and filename. For example, %DEMO_DIR%\Limit Lines\Demo\filename.

Including a path substitution string in the filename ensures that the file will be saved in (or loaded from) the desired folder. Failure to do so may result either in a file created in an parent folder or a file error. Do not append a filename extension as the extension is automatically added.

Example Command Sequence

:LLINe2:LOAD:FNAMe "%USER_DATA_DIR%\Limit Lines\LimitLine.lltx"
:LLINe2:DISPlay ON